SPRADN0 December 2024 F29H850TU , F29H859TU-Q1
After the UART flash kernel has been loaded onto the device RAM, a device firmware upgrade can be performed. This section discusses how to do this on a HS-FS device.
Figure 6-1 displays the options available when the flash kernel is running in RAM. For a firmware upgrade on an HS-FS device, select DFU CPU1 (option 1). After successful, select Run CPU1 (option 7) to branch from kernel to the newly loaded application. Alternatively, reset CPU1 (option 8) is also valid if the device is set to flash boot mode.