SPRADN0 December   2024 F29H850TU , F29H859TU-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Programming Fundamentals
  5. 2Introduction
    1. 2.1 Hardware Security Module
    2. 2.2 ROM Bootloader
    3. 2.3 Combined Image with X.509 Certificate
  6. 3Flash Kernel Implementation
    1. 3.1 CPU1 Firmware Upgrade (HS-FS)
    2. 3.2 Key Provision (HS-FS to HS-KP)
    3. 3.3 CPU1 Secure Firmware Upgrade (HS-KP/SE to HS-SE)
    4. 3.4 HSM Firmware Upgrade (HS-KP/SE to HS-SE)
    5. 3.5 SECCFG Code Provisioning (HS-KP/SE to HS-SE)
  7. 4Host Application: UART Flash Programmer
    1. 4.1 Overview
    2. 4.2 Build UART Flash Programmer with Visual Studio
    3. 4.3 Build UART Flash Programmer with CMake
    4. 4.4 Packet Format
    5. 4.5 Kernel Commands
  8. 5Example Usage
    1. 5.1 Loading the Flash Kernel onto the Device
      1. 5.1.1 Hardware Setup
      2. 5.1.2 Running the UART Flash Programmer
    2. 5.2 CPU1 Device Firmware Upgrade (HS-FS only)
    3. 5.3 Convert HS-FS to HS-SE
    4. 5.4 Loading a RAM-based HSMRt Image
    5. 5.5 Key Provision (HS-FS to HS-KP)
    6. 5.6 Code Provision (HS-KP/SE to HS-SE)
  9. 6Troubleshooting
    1. 6.1 General
    2. 6.2 UART Boot
    3. 6.3 Application Load
  10. 7Summary
  11. 8References

Application Load

Question: I can download the kernel to the device successfully, but I cannot successfully load the application to flash. What do I need to check?

Answer:

  • Make all sections in the linker cmd file that are allocated to flash are aligned to 512-bit boundaries. This can be done by adding palign(32) to the appropriate sections as shown below.
.text : {} > FLASH_RP0, palign(32)
  • Make sure there is an appropriate X.509 certificate in the first 0x1000 bytes of your binary file. Refer to Section 3.1 for specific instructions.