SPRUHM9H October 2014 – May 2024 TMS320F28075 , TMS320F28075-Q1 , TMS320F28076
When connected to the device using an emulator, the EMU_BOOTCTRL control word is used to determine the boot mode. This control word allows the user to experiment with various boot mode settings before writing to the BOOTCTRL register in the user-configurable DCSM OTP. The values that can be set in the BMODE field of the EMU_BOOTCTRL control word are listed in Section 4.7. Some notable options include being able to have emulation boot read from the boot mode select pins, emulate standalone boot using the values in OTP, and boot according to the Get boot value stored in OTP memory. Refer to Section 4.10.6 for details on the GPIOs used in the various boot modes.
| Key | BMODE Value | Realized Boot Mode |
|---|---|---|
| != 0x5A | Don’t Care | Wait Boot |
| 0xFE | Boot as per BMSP0 and BMSP1 | |
| 0xFF | Emulate Standalone boot | |
| 0x00 | Parallel Boot | |
| 0x01 | SCI Boot 0 | |
| 0x02 | Wait Boot | |
| 0x03 | Get Mode(read OTP BOOTCTRL) | |
| 0x04 | SPI Boot 0 | |
| = 0x5A | 0x05 | I2C Boot 0 |
| 0x07 | CAN Boot 0 | |
| 0x0A | RAM Boot | |
| 0x0B | Flash Boot | |
| 0x0C | USB Boot | |
| 0x81 | SCI Boot 1 | |
| 0x84 | SPI Boot 1 | |
| 0x85 | I2C Boot 1 | |
| 0x87 | CAN Boot 1 | |
| Other | Wait Boot |