SWCU185G January 2018 – June 2024 CC1312PSIP , CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
The FPU provides an extension register file containing 32 single-precision registers (see Figure 3-4). These can be viewed as:
Figure 3-4 FPU Register BankThe mapping between the registers is as follows:
For example, you can access the least significant half of the value in D6 by accessing S12, and the most significant half of the elements by accessing S13.