DLPU048E August 2016 – July 2024
The following configuration options are set in flash. The value of these parameters can be found in the flash header file that is provided along with the flash binary file.
| PARAMETER | DESCRIPTION |
|---|---|
| Alternate Source On Failure | Any test pattern or splash image to be displayed upon source loss. |
| Auto-recover | 0x0: Once the test fails, alternate source will continue to display even if the external source returns to a valid range. Host action is required to change to external source after failure.
0x1: If the test passes after failing, the system will return to displaying the external source. This does not require host action. |
| Pixel Clock maximum, minimum | Maximum and minimum allowable pixel clock frequency. This is generally set to ±2% of the nominal pixel clock. |
| VSYNC maximum, minimum | Maximum and minimum allowable VSYNC frequency. This is set to the VSYNC range specified in the DLPC230-Q1 data sheet. |
| Active Lines Per Frame | Vertical resolution of the external source. |
| Active Pixels Per Line | Horizontal resolution of the external source. |