DLPU048E August 2016 – July 2024
The DLPC230-Q1 includes an internal test pattern generator which can be used to display basic test images and verify system functionality without an external video source. Figure 5-5 through Figure 5-13 show the test patterns that may be generated.
Note that the test patterns below assume that the system uses red, green, and blue light sources. Test patterns displayed using single-color systems (including full-white light systems) may not appear as shown below.
Solid Color (White, Red, Green, Blue)
Figure 5-5 Test Pattern - Solid ColorColor Bars (8-color)
Figure 5-6 Test Pattern - Color BarsCheckerboard (White/Black)
Figure 5-7 Test Pattern - CheckerboardHorizontal Ramp (White/Black)
Figure 5-8 Test Pattern - Horizontal RampVertical Ramp (White/Black)
Figure 5-9 Test Pattern - Vertical RampGrid Lines (White, Black)
Figure 5-10 Test Pattern - Grid White
Figure 5-11 Test Pattern - Grid BlackDiagonal Lines (White, Black)
Figure 5-12 Test Pattern - Diagonal White
Figure 5-13 Test Pattern - Diagonal Black