DLPU099B May 2018 – November 2025
The DLP5531-Q1 Electronics EVM kit contains the following cables, see Figure 1-3.
| NAME | REFERENCE | QUANTITY |
|---|---|---|
| Cheetahâ„¢ SPI Host Adapter | A | 1 |
| Host SPI Cable | B | 1 |
| Host I2C Cable (Includes PROJ_ON, HOLD_BOOT, HOST_IRQ signals) | C | 1 |
| Headlight Driver Interface Cable | D | 1 |
| LED Power Cable | E | 3 |
| Formatter Power Cable | F | 1 |
| Input Power Cable | G | 1 |
| Micro HDMI Cable | H | 1 |
| OpenLDI Flex Cable | I | 1 |
| Fan Power Cable | J | 3 |
Figure 1-3 Cables Included in DLP5531-Q1 Electronics EVM