A diagram of all connections is shown in Figure 2-1.
- Connect the Headlight Driver Interface cable to the Formatter Board (J10) and the LED Driver Board (J4).
- Connect the Host SPI cable to the Formatter Board (J2) and the Cheetah adapter. Connect the Cheetah adapter’s USB cable to PC.
- Connect the Formatter Power cable to the Formatter Board (J11) and the LED Driver Board (J1).
- Connect the LED power cable to any of the LED Driver Board LED ports (J7, J8, J9). Note that some ports may be disabled by flash setting. LED 0 (J7) is used by default.
- Connect the Fan Power cable to any of the LED Driver Board fan ports (J3, J5, J6). Confirm the fan switch on the LED Driver Board (SW1) is in the ON position.
- Connect the Micro HDMI cable to the Formatter Board (J3). Connect the Micro HDMI cable to PC HDMI port.
- Connect the Power Input cable to the LED Driver Board (J2).