- Using the DLPC230-Q1 Automotive Control Program, which is connected to the EVM, navigate to the "Flash Program" tab.
- Using the folder icon, select an Image File (.bin) and open it.
- Click "Program and Verify Flash Memory."
Note that if the device is in Display mode, it will automatically be switched to Standby during programming.