An example image of the DLP4620SQ1EVM
without a power supply and optics is shown in Figure 3-1.
- Connect the DMD Flex Cable to the controller PCB (J1) and the DMD PCB
(J1). Pin 1 is marked on the DMD flex cable. Make sure the controller side of the flex
cable is aligned with the controller PCB.
- Connect the controller to driver control interface flex to the
controller PCB (J8) and the illumination driver PCB (J4).
- Connect your host communication cable to the controller PCB and your
host computer.
- If using the Total Phase Cheetah SPI Adapter, follow the jumper
configuration found in Section 3.4.
- If using a direct USB connection, then follow the jumper
configuration found in Section 3.5.
- Connect the controller power cable to the controller PCB (J5) and the
illumination driver PCB (J3).
- Connect the blue illumination output cable to the illumination driver
PCB (J5) to the blue illuminator in the optics engine.
- Connect the green illumination output cable to the illumination driver
PCB (J6) to the green illuminator in the optics.
- Connect the red illumination output cable to the illumination driver PCB
(J7) to the red illuminator in the optics engine.
- Connect the photodiode cable to the controller PCB (J7) to a photodiode
located in the illumination path of the optics engine.
- Connect the HDMI cable to the controller PCB (J4). Connect the HDMI
cable to PC HDMI port.
- Connect the power input cable to the illumination driver PCB (J1).