SBAA383C January 2020 – January 2024 TLV320ADC3120 , TLV320ADC3140 , TLV320ADC5120 , TLV320ADC5140 , TLV320ADC6120 , TLV320ADC6140
When PurePath Console is launched, it queries the user on how many devices are connected to an AC-MB, as shown in Figure 4-3. In this dialog window, after selecting two TLV320ADC5140 devices and clicking on Next, the main window shown in Figure 4-4 launches.
Figure 4-3 PurePath Console Input Number of Devices DialogPurePath Console configures only one device at a time. The devices are labeled by a device icon with a letter at the top of the screen, as shown in Figure 4-4. Clicking on device icon A programs the lower number I2C address, B programs the next I2C address, and so forth.
Figure 4-4 PurePath Console Main
WindowThe Audio Serial Bus tab assigns each channel of a device to a slot. In Figure 4-5, the device A input channels 1-4 are assigned to slots 0-3, respectively. In Figure 4-6, the device B input channels 1-4 are assigned to slots 4-7. Note that the previous slots in the TDM bus are not shown, but an ellipsis at the beginning of the audio interface signal line plot in BCLK, FSYNC, and SDOUT signifies that other slots precede these slots.
Figure 4-5 PurePath Console Device A
Channel to Slot Mapping
Figure 4-6 PurePath Console Device B
Channel to Slot MappingClicking on the upper right window expansion icon of the Audio Serial Bus graphic shows all slots and all devices, as shown in Figure 4-7.
Figure 4-7 PurePath Console Channel to
Slot Mapping for Device A and B