SBAA520A July 2021 – December 2025 ADS117L11 , ADS127L11 , ADS127L14 , ADS127L18 , ADS127L21 , ADS127L21B
The ADS1x7Lxx multichannel ADCs use a dedicated frame-sync data port for conversion results that is separate from the SPI port. Instead, the SPI port is only used to read and write register configuration data. However, similar to SPI, the frame-sync data port can also be connected in a daisy-chain configuration.
The frame-sync data port for the ADS1x7Lxx multichannel family operates in controller mode such that the ADC generates both the data clock (DCLK) and the word clock (FSYNC). Additionally, the ADC can provide data on 1, 2, or 4 data-lanes (DOUT0, DOUT1, DOUT2, and DOUT3) in a daisy-chain configuration. While using all 4 data-lanes does help increase the throughput, this method comes at the cost of requiring more physical connections to the ADC.
To use frame-sync daisy-chain mode, the DP_DAISY bit in DP_CFG1 register must be set to 0b, which is also the default value. In this configuration (1, 2, or 4 data lanes), DINx data are shifted in and appended to the original channel data. Refer to the ADS1x7Lxx family data sheet for additional details.
Similar to SPI daisy-chain, frame-sync daisy-chain effectively links individual ADC shift registers into longer length registers. Figure 10-1, Figure 10-2, and Figure 10-3 illustrates these configuration options for 1, 2, and 4 data lanes, respectively.
Using a daisy-chain connection reduces the number of IO pins needed on the host controller and simplifies the routing of the board. The daisy-chain frame-sync signals include 1 DCLK line, 1 FSYNC line, and 1, 2, or 4 DOUT lines. In addition to the frame-sync signals, a common CLK and START signal are needed for proper synchronization. Additional hardware lines can be used as well, especially if using Hardware Programming mode.
Figure 10-4, Figure 10-5, and Figure 10-6 show the frame-sync daisy-chain connections for one-lane, two-lane, and four-lane configurations, respectively. Note that only one FSYNC and one DCLK connection to the frame-sync receiver is needed because all ADCs are synchronized for daisy-chain and all FSYNC and DCLK signals have the same frequency and phase.
Select the desired number of data lanes by writing to the DP_TDM[1:0] field in the DP_CFG1 register. Figure 10-7 shows a typical ADS1x7L18 data transfer for the one data-lane configuration shown in Figure 10-4. See the ADS1x7Lxx family data sheets for additional details regarding these configurations and the resulting data output sequence.