SBAA634A April   2026  – September 2026 TAA5212 , TAA5412-Q1 , TAC5111 , TAC5111-Q1 , TAC5112 , TAC5112-Q1 , TAC5211 , TAC5212 , TAC5311-Q1 , TAC5312-Q1 , TAC5412-Q1 , TAD5112 , TAD5112-Q1 , TAD5212 , TAD5212-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Detailed Description
    1. 2.1 Common Mode Tolerance Modes
    2. 2.2 Common-Mode Rejection
    3. 2.3 Device Performance Across CM_TOL Modes
  6. 3Summary
  7. 4References
  8. 5Revision History

Introduction

Figure 1-1 (a) describes a differential-input amplifier, with input signals VIN+ and VIN- on the (+) and (-) terminals respectively.

 Differential-Input AmplifierFigure 1-1 Differential-Input Amplifier

For an ideal amplifier, the output VOUT is:

Equation 1. VOUT=Ad*(VIN++VIN-)

Where Ad is the differential gain of the amplifier.

However, in a practical amplifier, mismatches between the (+) and (-) signals paths can result in an additional component to the output signal. To compute this, the circuit in Fig 1-1 (b) can be equivalently represented as shown in Figure 1-1 (b), with a "differential signal" VDIFF, and a "common-mode" signal "VCM". For such an amplifier, the output is given by:

Equation 2. VOUT=Ad*VDIFF+Ac*VCM

Where Ad is the differential gain, and Ac is called the common-mode gain of the amplifier. These signals are given by:

Equation 3. VDIFF=VIN+-VIN-
Equation 4. VCM=VIN++VIN-2

One of the key performance parameters for a differential input system is it's ability to "reject" such common-mode signals. This is called "Common-Mode Rejection Ratio (CMRR)", and the value of CMRR in dB is given by:

Equation 5. CMRRdB=20*log⁡(1Ac)

For an ideal differential amplifier, the CMRR is ∞ dB.

The CMRR of a non-ideal amplifier can be measured by providing the same signal VCM at both the input terminals and observing the output VOUT. The CMRR can then be calculated as:

Equation 6. CMRRdB=20*log⁡VCMVOUT

However, such circuits also have a specified range of common-mode swing which they can tolerate. In this document, the common-mode swing tolerance for the TAC5x1x/TAC5x1x-Q1 devices is discussed, along with how this tolerance can be programmed, and its impact on device performance.