To operate the GUI, follow these steps:
- Connect to and launch the GUI as
described in Section 5.1.3.1.
- Close the README.md file page that
pops up after the EVM connects to the GUI. The text near the bottom-left hand
corner of the GUI reads Hardware Connected.
- If Hardware
Connected does not show in the bottom-left hand corner of the
GUI, then check different hardware COM ports under Options → Serial
Port.
- If the hardware still does
not connect, make sure you are using the correct GUI and EVM
combination.
- Click the Registers icon to
open the Registers page (also available on the left-side menu). Note that
the registers listed are not registers on the TMAG5328 but are internal
variables stored in the microcontroller that are not directly used for EVM
evaluation. These variables cannot be modified from the Registers page
and can be ignored.
- At the top of the Registers
page, change Auto Read to As fast as possible.

The TMAG5328 also has a Results page for viewing the state of the TMAG5328 OUT
pin and a DAC configuration page for configuring the DAC. Both of these pages
are described in the sections below.