SBAU376A December   2021  – March 2022

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Overview
    1. 1.1 Features
  5. 2Kit Contents
  6. 3Related Documentation From Texas Instruments
  7. 4Hardware
    1. 4.1 EVM Threshold Adjustment Options
      1. 4.1.1 Adjusting Threshold With DAC
      2. 4.1.2 Adjusting Threshold With Potentiometer
        1. 4.1.2.1 Using the Potentiometer to Estimate the Magnetic Flux Density Sensed by the TMAG5328
      3. 4.1.3 Adjusting Threshold With Fixed Resistor
    2. 4.2 Power Supply Options and Jumper Settings
  8. 5EVM Operation
    1. 5.1 Evaluation With SCB and GUI
      1. 5.1.1 Driver Installation
      2. 5.1.2 Firmware
        1. 5.1.2.1 Updating Firmware on SCB
      3. 5.1.3 GUI Setup and Usage
        1. 5.1.3.1 Initial Setup
        2. 5.1.3.2 GUI Operation
          1. 5.1.3.2.1 GUI Results Page
          2. 5.1.3.2.2 GUI DAC Configuration Page
      4. 5.1.4 Direct EVM Serial Communication
    2. 5.2 Evaluation Without SCB and GUI (EVM Stand-Alone Mode)
    3. 5.3 Head-On Linear Displacement Demo
  9. 6Schematics, PCB Layout, and Bill of Materials
    1. 6.1 Schematics
    2. 6.2 PCB Layout
    3. 6.3 Bill of Materials
  10. 7Revision History

Evaluation Without SCB and GUI (EVM Stand-Alone Mode)

The TMAG5328EVM can operate in a stand-alone mode that does not require the SCB or GUI. To operate in stand-alone mode, an external power supply must be connected to the TMAG5328EVM (see Section 4.2).

When in standby mode, BOP can be set using either the DAC, potentiometer, or fixed resistor options. Remember that the DAC output voltage cannot be changed without the SCB. The DAC output voltage will only be set to the value that was previously stored in its nonvolatile memory by the GUI. As a result, the DAC cannot be swept to find the sensed magnetic flux density of the TMAG5328 unless the SCB is connected. The potentiometer, however, does not require the SCB to estimate the sensed magnetic flux density TMAG5328 (see Section 4.1.2.1).

When in stand-alone mode, the TMAG5328 OUT pin can be probed at the test point that is labeled "OUT" on the board or on pin 9 of header J1. In addition, LED D1 can be used to visually observe the state of the TMAG5328 OUT pin. Figure 5-21 shows the LED circuit connected to the OUT pin on the TMAG5328. If OUT is asserted high, the LED is OFF. If OUT is asserted low, the LED is ON.

GUID-20211108-SS0I-LCL1-KPMB-QLCSVBXBRBPP-low.pngFigure 5-21 OUT LED Circuit.