SBAU376A December 2021 – March 2022 TMAG5328
Click the Results Data icon
to view the Results
page. This screen shows the state of the TMAG5328 OUT pin. Remember to set the
Auto Read option on the Registers page to As fast as
possible to view the results on this pin (see Section 5.1.3.2).
Figure 5-9 shows an example plot of the OUT waveform. If the TMAG5328 OUT pin is at a high state (LED is OFF), a "1" is displayed on the graph. If the pin is at a low state (LED is ON), a "0" is displayed on the graph. The number of samples stored in the plot can be modified by adjusting the "1000" at the top of the screen with the desired number of samples then clicking enter. In addition, the plot can be exported by clicking the SAVE PLOT button.
Figure 5-9 TMAG5328 GUI Results
Page