SBAU430 April   2025

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents (Required Equipment)
  6. 2Hardware
    1. 2.1 Setup Procedure
      1. 2.1.1  Installing the DAC39RF12EVM Configuration GUI Software
        1. 2.1.1.1 Installing & Setting Up Vivado Lab Tools
      2. 2.1.2  Connect the DAC39RF12EVM and TSW14J59EVM
      3. 2.1.3  Connect the Power Supplies to the Boards (Power Off)
      4. 2.1.4  Connect the Spectrum Analyzer to the EVM
      5. 2.1.5  Turn On the TSW14J59EVM Power and Connect to the PC
      6. 2.1.6  Turn On the DAC39RF12EVM Power Supplies and Connect to the PC
      7. 2.1.7  Turn On the Signal Generators
      8. 2.1.8  Launching the DAC39RF12EVM GUI and Programing the DAC EVM - JMODE 0
      9. 2.1.9  Launching the DAC39RF12EVM GUI and Programing the DAC EVM - JMODE 1
      10. 2.1.10 Launching the DAC39RF12EVM GUI and Programing the DAC EVM - JMODE 3
    2. 2.2 Evaluation Board Details: Analog Outputs
    3. 2.3 FMC Signal Routing
  7. 3References
    1. 3.1 Trademarks

Connect the Power Supplies to the Boards (Power Off)

  1. Confirm the power switch on the TSW14J59EVM is in off position. Connect the power cable to a 12V DC (minimum 5A) power supply. Make sure the proper supply polarity by confirming the outer surface of the barrel connector is GND and the inner portion of the connector is 12V. Connect the power cable to the TSW14J59EVM power connector.
  2. DAC39RF12EVM can be powered with 12V DC (minimum 3A) though the connector jack(J5) on the DAC39RF12EVM, or the EVM can be powered from the TSW14J59EVM via FMC+ connector. There is a switch (SW1) which can be used to select power from the barrel jack on the DAC EVM, or from TSW14J59EVM through FMC+ connector. Confirm that the power switch for the DAC39RF12EVM power supply is set to the opposite position (Jack) from which it should be drawing power. If using barrel jack option, connect the power cable to a 12V DC (minimum 3A) power supply. Make sure the proper supply polarity by confirming that the outer surface of the barrel connector is GND and the inner portion of the connector is 12V. Connect the power cable to the EVM power connector. Table 2-1 is used as a reference to power the DAC EVM.
Table 2-1 Powering the DAC39RF12EVM
DAC39RF12 Powered fromDAC39RF12 Power Switch positionTSW14J59EVM FMC switch positionPower supply needed
TSW14J59EVM via FMC+ connectorFMCON12V 5A for TSW14J59EVM
External Supply with jack on DAC39RF12EVMJACKOFF12V 3A for TSW14J59 and 12V 3A for DAC39RF12EVM
CAUTION: Make sure the power connections to the EVMs are the correct polarity. Failure to do so may result in immediate damage. Leave the power switches in the off position until directed later.