SBOA626 December   2025 OPA187 , OPA192 , OPA202 , OPA320

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Simple Analogy Explaining Instability
    2. 1.2 Circuits With Possible Stability Issues
    3. 1.3 Simple Stability Correction Based on Datasheet Plots
    4. 1.4 Introducing Lab Tools and Measurements
  5. 2Stability Theory for Operational Amplifiers
    1. 2.1 Poles and Zeros
    2. 2.2 Operational Amplifier Model Requirements for Stability Verification
    3. 2.3 Stability Definitions Based on Control Loop Model
    4. 2.4 Graphing Loop-Gain Based on AOL and 1/β
    5. 2.5 Rate of Closure Stability Test
    6. 2.6 Indirect (Non-Invasive) Stability Tests
  6. 3Simulating Open-Loop Stability Tests
    1. 3.1 Breaking the Loop the Wrong Way
    2. 3.2 Breaking the Loop With LC Test Circuit
    3. 3.3 Differential Loop Break Test
  7. 4Stability Correction for Capacitive Load
    1. 4.1 Isolation Resistor (RISO) Method
    2. 4.2 Dual Feedback Method
      1. 4.2.1 RISO-Dual-Feedback With RL
      2. 4.2.2 Dual Feedback With RFX Method
    3. 4.3 Snubber Circuit for Compensating Power Amplifiers and Reference Drive
    4. 4.4 Noise Gain for Stability Compensation
    5. 4.5 Feedback Capacitor (CF) Compensation for Capacitive Load
  8. 5Stability Corrections for Capacitance on the Inverting Node
    1. 5.1 Input Capacitance Instability Due to Zero in 1/β
    2. 5.2 Feedback Capacitor Solves Stability Issue for Capacitance on the Inverting Node
    3. 5.3 Minimum, Balanced, and Maximum Feedback Capacitance
    4. 5.4 Transimpedance Case
  9. 6Complex Open-Loop and Closed-Loop Output Impedance
    1. 6.1 Converting Open-Loop Output Impedance to Closed-Loop Output Impedance
    2. 6.2 Open-Loop and Closed-Loop Model Test
    3. 6.3 Instability Due to Resonance From Complex Output Impedance
    4. 6.4 Impact of Internal Op Amp Topology on Output Impedance Versus Frequency
    5. 6.5 Other Factors Effecting Output Impedance
  10. 7AOL Impact on Stability
    1. 7.1 AOL Secondary Poles and Zeros
    2. 7.2 Modeling the AOL Secondary Poles and Zeros and Input Capacitance
    3. 7.3 Decompensated Op Amps and Stability
    4. 7.4 The Impact of Closed-Loop Gain on Stability
  11. 8Common Problems in Stability Analysis
  12. 9References

Simple Analogy Explaining Instability

Figure 1-1 illustrates an op amp circuit with stability issues and an equivalent control system diagram. Control system diagrams and control system terminology are often used in op amp stability discussions because much of the literature for stability was developed for control systems and then applied to op amp circuits. The inputs of the op amp correspond to the following blocks for the summing block of the control system:

  • The amp open-loop gain (AOL) is the control system gain block.
  • The op amp feedback network corresponds to the beta feedback block (β).
OPA187 OPA202 OPA320 OPA192 Operational Amplifier Circuit
                    and Control System Equivalent Figure 1-1 Operational Amplifier Circuit and Control System Equivalent

The circuit in Figure 1-1 is unstable because of the delay elements in the feedback network. The delay elements are simply RC low pass filters. A low pass filter naturally has a group delay or phase shift. The reason that this feedback delay causes instability can be understood by thinking of the op amp circuit as a control system. The input summing block of the op amp senses the output signal through the feedback network. The output of the summing block is the error signal. In this example, the target for VOUT is 2 × VIN. When VOUT = 2VIN the error signal is zero. When the output is too high (VOUT > 2 × VIN), the error signal is negative and the op amp tries to drive the output downward. Similarly, when the output is too low (VOUT < 2 × VIN), the error signal is positive and the op amp tries to drive the output upward to cancel the error. Thus, the output is a constant value of VOUT = 2VIN when the system is in equilibrium.

However, the functionality of the system assumes the feedback signal (VFB) is not significantly delayed. If VFB is significantly delayed, the op amp can incorrectly identify the output as going upward when the output is actually going downward. This outcome creates an error signal with the wrong polarity, which drives the output in the wrong direction. Instability of the op amp is caused by this delay in the feedback signal.

Many engineers see the circuit shown in Figure 1-1 and understand that the feedback delay is a problem, and the general assumption is no one intentionally designs such an impractical circuit. However, the circuit shown in Figure 1-1 is frequently inadvertently created by the internal open-loop output impedance (RO or ZO), the input capacitance of the op amp, and any parasitic PCB capacitance (CIN = CCM+CPCB). Figure 1-2 shows the circuit redrawn to emphasize how the delay elements are created in a practical op amp circuit.

OPA187 OPA202 OPA320 OPA192 Origin of Delay Elements in a
                    Practical Circuit Figure 1-2 Origin of Delay Elements in a Practical Circuit