SBOA626 December   2025 OPA187 , OPA192 , OPA202 , OPA320

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Simple Analogy Explaining Instability
    2. 1.2 Circuits With Possible Stability Issues
    3. 1.3 Simple Stability Correction Based on Datasheet Plots
    4. 1.4 Introducing Lab Tools and Measurements
  5. 2Stability Theory for Operational Amplifiers
    1. 2.1 Poles and Zeros
    2. 2.2 Operational Amplifier Model Requirements for Stability Verification
    3. 2.3 Stability Definitions Based on Control Loop Model
    4. 2.4 Graphing Loop-Gain Based on AOL and 1/β
    5. 2.5 Rate of Closure Stability Test
    6. 2.6 Indirect (Non-Invasive) Stability Tests
  6. 3Simulating Open-Loop Stability Tests
    1. 3.1 Breaking the Loop the Wrong Way
    2. 3.2 Breaking the Loop With LC Test Circuit
    3. 3.3 Differential Loop Break Test
  7. 4Stability Correction for Capacitive Load
    1. 4.1 Isolation Resistor (RISO) Method
    2. 4.2 Dual Feedback Method
      1. 4.2.1 RISO-Dual-Feedback With RL
      2. 4.2.2 Dual Feedback With RFX Method
    3. 4.3 Snubber Circuit for Compensating Power Amplifiers and Reference Drive
    4. 4.4 Noise Gain for Stability Compensation
    5. 4.5 Feedback Capacitor (CF) Compensation for Capacitive Load
  8. 5Stability Corrections for Capacitance on the Inverting Node
    1. 5.1 Input Capacitance Instability Due to Zero in 1/β
    2. 5.2 Feedback Capacitor Solves Stability Issue for Capacitance on the Inverting Node
    3. 5.3 Minimum, Balanced, and Maximum Feedback Capacitance
    4. 5.4 Transimpedance Case
  9. 6Complex Open-Loop and Closed-Loop Output Impedance
    1. 6.1 Converting Open-Loop Output Impedance to Closed-Loop Output Impedance
    2. 6.2 Open-Loop and Closed-Loop Model Test
    3. 6.3 Instability Due to Resonance From Complex Output Impedance
    4. 6.4 Impact of Internal Op Amp Topology on Output Impedance Versus Frequency
    5. 6.5 Other Factors Effecting Output Impedance
  10. 7AOL Impact on Stability
    1. 7.1 AOL Secondary Poles and Zeros
    2. 7.2 Modeling the AOL Secondary Poles and Zeros and Input Capacitance
    3. 7.3 Decompensated Op Amps and Stability
    4. 7.4 The Impact of Closed-Loop Gain on Stability
  11. 8Common Problems in Stability Analysis
  12. 9References

Dual Feedback Method

Figure 4-12 illustrates the main disadvantage of the RISO method. When an amplifier with an isolation resistance drives a resistive load, a voltage divider is formed. The voltage divider attenuates the amplifier output at the load:

Equation 29. VOUT=VO×RL/RL+RISO

The graph in Figure 4-12 shows that the 10mV step input is attenuated by 2.67mV at the output. The attenuation is a gain error that can be calibrated out if the load resistance is well controlled, but this is not practical in some cases. The RISO-dual-feedback topology eliminates the voltage divider effect seen in the RISO method by using an output sense feedback path. Figure 4-13 shows the RISO-dual-feedback implementation with the same op amp and capacitive load as Figure 4-5. Notice that VOUT on the RISO-dual-feedback circuit settles to the same voltage as the input signal. The amplifier output (VO in Figure 4-13) settles to a voltage greater than the input signal to compensate for the drop across RISO. The voltage swing of the RISO-dual-feedback circuit at the load (RL) is limited by the voltage drop across RISO.

OPA187 OPA202 OPA320 OPA192 RISO Voltage Attenuation at the LoadFigure 4-12 RISO Voltage Attenuation at the Load
OPA187 OPA202 OPA320 OPA192 RISO-Dual-Feedback Voltage at Load Equal to Input (VS = VOUT)Figure 4-13 RISO-Dual-Feedback Voltage at Load Equal to Input (VS = VOUT)

At low frequencies, the impedance of a capacitor can be considered an open circuit, and at high frequencies the impedance is a short circuit:

Equation 30. XC=1/2×π×f×C

The RISO-dual-feedback circuit operation can be understood by considering the low and high-frequency operation separately (see Figure 4-14). At low frequency, the feedback capacitor is open and the feedback resistor RF senses the output VOUT. The op amp adjusts the output VO until VO = VOUT. For the DC circuit, the voltage on the inverting and non-inverting input are equal due to the virtual short. Since there is no current flowing through RF, there is no drop across RF so VOUT = VINV = VS. At high frequencies, the feedback capacitor CF acts like a short. Compared to the low impedance of the CF capacitor at high frequency, the feedback resistor is an open circuit. For the high frequency operation, the circuit looks the same as the RISO circuit. Thus, for a low frequency operation, the feedback resistor forces the output to be equal to the source voltage, and for a high frequency operation, the isolation resistance provides stability for the capacitive load.

OPA187 OPA202 OPA320 OPA192 AC and DC Operation of RISO-Dual-Feedback ConfigurationFigure 4-14 AC and DC Operation of RISO-Dual-Feedback Configuration

RISO-Dual-Feedback design method illustrates the step-by-step method for choosing the components for the RISO-dual-feedback topology. First, select RISO using the same methods explained in RISO conservative design method or RISO design method for minimum RISO. Second, choose RF to be at least 100 times larger than RISO. Setting RF greater than RISO makes RF effectively open in the AC case (see Figure 4-14). Finally, choose CF according to Equation 31. Check the transient and AC response and adjust CF within the bounds of the inequality given in Equation 32 to improve the response. The derivation of the inequality is covered in Equation 31 and Equation 32.

Note: RISO-Dual-Feedback Design Method
  1. Select RISO using the RISO conservative design method or RISO design method for minimum RISO.
  2. Set RF ≥ 100 × RISO.
  3. Set CF according to Equation 31.
Equation 31. CF=4×RISO×CLRF
Equation 32. 2×RISO×CLRF≤CF≤10×RISO×CLRF

The values for Figure 4-15 were derived using RISO-Dual-Feedback design method and rounded to standard resistor and capacitor values. This example uses the same amplifier from Figure 4-5. The nominal value for CF is 180pF from Equation 31. CF can be adjusted from 90pF to 905pF according to Equation 32 to improve settling and overshoot. This circuit is used throughout this section for transient and open-loop discussions.

OPA187 OPA202 OPA320 OPA192 RISO-Dual-Feedback Configuration From Design ProcedureFigure 4-15 RISO-Dual-Feedback Configuration From Design Procedure

The design procedure in RISO-Dual-Feedback design method uses the inequality in Equation 32 to select the feedback capacitor. This inequality is used to prevent a resonance in the feedback network. To understand this potential resonance, splitting the feedback network into two paths using superposition is useful. Figure 4-16 and Figure 4-17 illustrate the two feedback paths. Each path constitutes a 1/β, and the combined 1/β is the minima of the two separate paths. The minima of the two paths are used to combine the two 1/β because the two 1/β are in parallel and the lowest impedance in parallel dominates.

The feedback path through RF is separated from the overall feedback network by opening CF (see FB1 in Figure 4-16). FB1 is a simple RC filter that generates a zero in 1/β1 (see Equation 33). The transfer function for 1/β1 approaches 0dB and low frequency and increases at 20dB per decade at high frequency. Equation 35 shows the zero frequency, where 1/β1 is +3dB. The feedback through CF is separated from the overall feedback network by opening RISO (see FB2 in Figure 4-17). For this analysis we assume that the capacitive reactance of CL is very low so that the reactance acts as a short. The transfer function of 1/β2 has both a pole and a zero (see Equation 34). The pole is located at 0Hz, so the function continuously rolls off at 20dB/decade for low frequency. At higher frequency, the pole is canceled by the zero, so 1/β2 flattens out at approximately 0dB. The zero frequency for FB2 is given in Equation 36. Figure 4-18 illustrates 1/β1, 1/β2, and the combined 1/β. Since both feedback paths contain complex numbers, the combined 1/β do not linearly add as there is some calculation in the complex addition. Notice that the combined 1/β shows a resonant peak where the two 1/β functions cross. This resonance can cause instability if the inequality in Equation 32 is not followed.

OPA187 OPA202 OPA320 OPA192 Superposition of Feedback Paths for 1/β (Feedback Through RF)Figure 4-16 Superposition of Feedback Paths for 1/β (Feedback Through RF)
OPA187 OPA202 OPA320 OPA192 Superposition of Feedback Paths for 1/β (Feedback Through CF)Figure 4-17 Superposition of Feedback Paths for 1/β (Feedback Through CF)
OPA187 OPA202 OPA320 OPA192 1/β for Both Feedback Paths and Combined 1/βFigure 4-18 1/β for Both Feedback Paths and Combined 1/β
Equation 33. 1β1=VOVFB1=s1/RISO×CL+1
Equation 34. 1β2=VOVFB2=RF×CF+1RF×CF×s
Equation 35. fFB1=12×π×RISO×CL
Equation 36. fFB2=12×π×RF×CF

The resonance in 1/β occurs when the 3dB points on 1/β1 and 1/β2 are too close together. For example, if the 3dB point on 1/β2 is much lower than the 3dB point on 1/β1, then the two curves combine to form a relatively flat 1/β. Conversely, when the two 3dB points are close together, the two curves combine to form a resonant peak in 1/β (see Figure 4-19). This relationship between the cutoff frequencies determines the basis for the inequality (see Equation 37 through Equation 40 for derivation). Inspecting Figure 4-19, you can graphically see that fCB1 > fCB2 minimizes resonant peaking (see Equation 37 and Equation 38). To complete this derivation, remember that taking the reciprocal on both sides of the inequality flips the inequality sign for positive numbers (see Equation 39). Dividing by 2 × π × RF yields Equation 40. Based on empirical results, CF must be at least two times CL × RISO / RF to avoid instability due to the resonance. The factor of 10 for the maximum value of CF was selected empirically to achieve a reasonable settling time. Technically, a larger factor can be used but then the settling is unnecessarily long.

OPA187 OPA202 OPA320 OPA192 Impact of 3dB Spacing on 1/β Curves for Resonant PeakingFigure 4-19 Impact of 3dB Spacing on 1/β Curves for Resonant Peaking
Equation 37. fCFB1>fCFB2
Equation 38. 12×π×RISO×CL>12×π×RF×CF
Equation 39. 2×π×RISO×CL<2×π×RF×CF
Equation 40. CF>RISO×CLRF

The transient response of the circuit from Figure 4-15 is simulated in Figure 4-20 across the range of CF from the design procedure. The target value of CF from the procedure is 362pF, but the range allows for CF from 90.5pF to 905pF. Figure 4-20 shows that the percentage overshoot is highest for the smallest capacitance, so if overshoot is a concern, choose a larger CF value. Figure 4-21 illustrates the same transient response with the axis scaled to illustrate a 0.1% settling time. Since the output settles to 5mV, the axis is adjusted to 5mV ± 0.01mV for 0.1% settling. In general, the settling time increases for larger values of CF. The exception to this trend happens for very low values of CF, where the feedback is starting to become resonant (181pF in this case). Thus, overshoot decreases for larger values of CF and settling time decreases. The recommended value of 362pF assumes the goal is for the shortest settling time while avoiding the resonance. See table Table 4-2 for a summary of settling time and overshoot versus CF.

OPA187 OPA202 OPA320 OPA192 RISO-Dual-Feedback Transient ResponseFigure 4-20 RISO-Dual-Feedback Transient Response
OPA187 OPA202 OPA320 OPA192 RISO-Dual-Feedback 0.1% Settling Transient ResponseFigure 4-21 RISO-Dual-Feedback 0.1% Settling Transient Response

Figure 4-22 illustrates the open-loop response for Figure 4-15. The portion of the curve where 1/β1 and 1/β2 intersect is magnified and shown for different values of CF. The phase response for different values of CF is also shown. Note that the highest magnitude of resonant peaking and most dramatic phase shift occurs for the smallest feedback capacitor. Notice that the resonance occurs at a frequency below the point where AOL intersects 1/β. Meaning, the resonance occurs below the point where phase margin is tested. This means that the resonance does not have a significant effect on phase margin. For circuits with very low CF, the resonance can cause instability even though the phase margin is good. Table 4-2 shows the settling time, percentage overshoot, and phase margin across the range of CF for Figure 4-15. Note that the phase margin looks good for all cases and shows no relationship to the percentage overshoot. This outcome is because phase shift from the resonance happens at a frequency below the phase margin test. Thus, instability due to the feedback resonance is not detected by the phase margin test. To avoid feedback resonance, adhere to the capacitance range in Equation 32 and inspect the 1/β curve for resonant peaking.

OPA187 OPA202 OPA320 OPA192 Open-Loop Dual-Feedback Response for Different CFFigure 4-22 Open-Loop Dual-Feedback Response for Different CF
Table 4-1 RISO-Dual-Feedback Transient Summary
CF (pF)0.1% Settling (μs)Percent OvershootPhase Margin Open-Loop Test
90.538.254.795.0°
18132.135.391.0°
36225.619.789.1°
54348.113.988.5°
72464.710.888.1°
90578.08.688.0°

Inspecting the transient response in Figure 4-21 shows that graphs with low values of CF have a dampened sinusoidal oscillation, whereas graphs with low CF have an initial overshoot and a long settling tail. This settling behavior depends on whether the poles in the closed-loop transfer function are real or complex conjugates. The transfer function for a system with complex conjugate poles is given in Equation 41 and the transient step response is given in Equation 42. Note that the transient step response for complex poles is an exponentially dampened sinusoidal function. The transfer function for a system with two real poles is given in Equation 43 and the transient step response is given in Equation 44. The transient step response for real poles contains two exponential functions with two different time constants. Normally, the exponential with the short time constant has a large coefficient that corresponds to the overshoot. The exponential with the short time constant has a coefficient that cancels the other exponential when settled (5-time constants). The combination of the two exponentials produces a large overshoot with a long settling tail. Thus, for the dual-feedback circuit, large values of CF produce the smallest overshoot but have the longest settling tail (see Figure 4-23). From a practical perspective, the response with the dampened sinusoidal waveform is an indication of instability, whereas the single overshoot with a long settling tail indicates two real poles. The main concern with the system containing two real poles is that the long settling time limits the accuracy and speed of the system (see Demystifying pole-zero doublets).

Equation 41. GIs=ωn2s2+2ζωns+ωn
Equation 42. L-1GIs×1s=1-e-ζωntcos⁡ωdt-ζ1-ζ2sin⁡ωdt
Equation 43. GRs=1+s/ωz1+s/ω11+s/ω2×1s
Equation 44. L-1GRs×1s=1-V1e-ω1t-V2e-ω2t
OPA187 OPA202 OPA320 OPA192 Step Response for Complex Versus Real PolesFigure 4-23 Step Response for Complex Versus Real Poles