SBOA626 December 2025 OPA187 , OPA192 , OPA202 , OPA320
Figure 3-3 illustrates the SPICE test circuit used to generate the open-loop output impedance graph. The circuit uses a large 1TH test inductor in the feedback path to create a closed-loop DC bias path, but an open-loop response for AC frequencies. The current source at the output injects a current into the output impedance so that the output voltage is equal to the output impedance. When displaying the response in SPICE, make sure to display the results as a linear value on a logarithmic scale and not in decibels. Figure 6-5 shows that the simulated ZO compares well to the measured ZO as specified in the OPA189 data sheet. The correct modeling of ZO is critical for doing stability testing, so confirming the model accuracy using this test method is important. Note that the vast majority of Texas Instruments op amp models have an accurate ZO model.
Figure 6-6 illustrates how to test closed-loop output impedance versus frequency. For this test, inject a test current and monitor the output voltage. The example shows a unity gain configuration, but the test must be done in whatever gain is used in the application. The simulated output voltage is equal to the closed-loop output impedance. Make sure to display the results as a linear value on a logarithmic scale and not in decibels.
Figure 6-7 compares the closed-loop and open-loop output impedance for the OPA189. The OPA189 is an interesting example because the open-loop impedance is not flat across frequency. Rather, the OPA189 open-loop impedance has multiple different regions where the impedance acts inductive, capacitive, or resistive. Recall that the impedance of an inductor increases at 10x/dec (ZL = j × 2 × π × f × L), and the impedance of a capacitor decreases at 10x/dec (ZC = 1/(j × 2 × π × f × C). In this open-loop graph example, notice that ZO increases from about 10Ω to 100Ω in one decade, so that region is called inductive. For the closed-loop plot, the slope of each region is increased by 10 times per decade, as discussed in Section 6. Thus, a capacitive region in open-loop becomes resistive in closed-loop because the capacitive pole is canceled by zero introduced in the translation from open-loop to closed-loop (see Figure 6-7). Likewise, resistive open-loop impedance translates to inductive closed-loop, and inductive open-loop translates to double-inductive closed-loop. The term double inductive refers to the slope of 100x/dec in the closed-loop impedance. A double inductive slope can only be produced in a circuit with gain, as there are no physical double inductive circuit elements.