SBOK052 May 2024 OPA4H014-SEP
During SEL qualification, the device was heated using forced hot air, maintaining an IC temperature at 125°C. The temperature was monitored by means of a K-type thermocouple attached as close to the device as possible. The species used for the SEL testing was a silver (47Ag) ion with an angle-of-incidence of 0° for an LETEFF = 43MeV-cm2/mg. The kinetic energy in the vacuum for this ion is 1.634 GeV (15MeV/amu line). A flux of approximately 105 ions / cm2-s and a fluence of approximately 107 ions were used for two runs. The V+/V-supply voltage was supplied at the recommended maximum voltage setting of +/- 9V. Run duration to achieve this fluence was approximately two minutes. No SEL events were observed during all four runs listed in Table 5-1. Figure 5-1 shows a plot of the current versus time.
| Run # | Distance (mm) | Temperature (°C) | Ion | Angle | Flux (ions × cm2/mg) | Fluence (Number ions) | LETEFF (MeV × cm2/ mg) |
|---|---|---|---|---|---|---|---|
| 6 | 40 | 125 | Ag | 0° | 1.00E+05 | 1.00E+07 | 43 |
| 7 | 40 | 125 | Ag | 0° | 1.00E+05 | 1.00E+07 | 43 |
No SEL events were observed, which indicates that the OPA4H014-SEP is SEL-immune at LETEFF = 43MeV-cm2/ mg and T = 125°C. Using the MFTF method described in Appendix C and combining (or summing) the fluences of the two runs at 125°C (2 × 107), the upper-bound cross-section (using a 95% confidence level) is calculated in Equation 1:
Figure 5-1 Current vs Time (I vs t) Data
for V+ Current During SEL Run 6
Figure 5-2 Current vs Time (I vs t) Data
for V- Current During SEL Run 6
Figure 5-3 Current vs Time (I vs t) Data
for V+ Current During SEL Run 7
Figure 5-4 Current vs Time (I vs t) Data
for V- Current During SEL Run 7