SBOK052 May   2024 OPA4H014-SEP

 

  1.   1
  2.   OPA4H014-SEP Single-Event Latch-Up (SEL) Radiation Report
  3.   Trademarks
  4. 1Overview
  5. 2SEE Mechanisms
  6. 3Irradiation Facilities and Telemetry
  7. 4Test Device and Test Board Information
    1. 4.1 Qualification Devices and Test Board
    2. 4.2 Characterization Devices and Test Boards
  8. 5Results
    1. 5.1 SEL Qualification Results
    2. 5.2 SET Characterization Results: TAMU K500 Cyclotron
    3. 5.3 SEE Characterization Results: MSU FRIB Linac
    4. 5.4 Analysis
    5. 5.5 Weibull Fit
  9. 6Summary
  10.   A TAMU Results Appendix
  11.   B MSU Results Appendix
  12.   C Confidence Interval Calculations
  13.   D References

Characterization Devices and Test Boards

Heavy ions were used to irradiate the devices. A nominal flux of 1 × 105 ions / s-cm2 was used for SEL characterization, at 125°C die temperature. Nominal fluxes of 1 × 105 ions / s-cm2 to 5 × 105 ions / s-cm2 were used for SET characterization, at ambient temperature.

For SEE characterization, the OPA4H014-SEP was biased with split supplies. On all four channels, the inverting input was connected to the output as shown in Figure 4-3. Both a buffer condition and positive-gain condition were tested. Jumpers were used to modify the load resistance and change from G = 1 to G = 10. The default positions are shown.

 SEE Characterization Board
                    Schematic Figure 4-3 SEE Characterization Board Schematic
Input and supply voltages were provided by SMU PXI cards, connected with banana cables. A common input signal was applied to all channels. Figure 4-4 shows the decoupling capacitance scheme used on each board. Current was monitored over time for both V+ and V-. For SET testing, the device outputs were monitored using oscilloscope PXI cards, connected with BNC cables. 100Ω of series isolation resistance was used on each output channel to drive the cable capacitance.
 Characterization Board Decoupling Capacitances Figure 4-4 Characterization Board Decoupling Capacitances

An example of a decapped unit mounted on a characterization board is shown in Figure 4-5. The back side of the characterization board is shown in Figure 4-6. Note that despite silkscreen marking, 2kΩ resistors were used instead of 50Ω.

 Characterization Board
                    (Front) Figure 4-5 Characterization Board (Front)
 Characterization Board
                    (Back) Figure 4-6 Characterization Board (Back)