SBOSAL6A June 2025 – September 2025 XTR200
PRODUCTION DATA
The XTR200 operates over a supply voltage range of 8V to 60V. However, consider the environmental temperature, load current, and load resistance in the overall system design. Figure 7-15 shows the thermally-limited maximum supply voltage of the XTR200 over a range of PCB temperatures. Figure 7-15 shows a worst-case scenario of 22mA output current into a 0Ω load using the internal output transistor, IS and VG pins shorted.
The black curve shows the supply voltage resulting in a 125°C junction temperature (the maximum specified temperature of the XTR200) for the given PCB temperature. The red curve shows the supply voltages resulting in a 150°C junction temperature (maximum operating temperature of the XTR200) for a given PCB temperature. At approximately 150°C, the Error Flag pin (EF) voltage goes low, warning of high junction temperature.
The XTR200 thermal shutdown circuitry disables the output for junction temperatures above 160°C. When the junction temperature falls back below 150°C, the output is re-enabled. For PCB temperatures below 70°C, the maximum recommended supply voltage is limited by the voltage rating of the XTR200 internal circuitry rather than thermal considerations. If high-temperature and high-supply-voltage operation is required, use an external transistor to deliver the load current as described in Using an External Transistor.
Consider the headroom specification of the XTR200 when determining the working power supply range of a system. The term headroom defines the difference between the supply voltage of the XTR200 and the load voltage as shown in Figure 7-16. Above the minimum supply voltage, 8V, confirm that the XTR200 supply voltage is at least 2.5V above the load voltage.