To set up the GUI the first time:
- Make sure that the proper driver is installed
successfully so that the GUI can update the EVM firmware, if necessary.
- Check to make sure the EVM/SCB Controller unit is plugged into the PC, then go to the previously-provided GUI link.
- Open the GUI Composer application to launch
the GUI from the web browser (see Figure 3-4).
- The GUI link brings up all
versions of the GUI. The newest version available is recommended.
- For first-time GUI Composer setup, follow the
prompts to download the TI Cloud Agent and browser extension (see
Figure 3-5). These prompts appear after closing the README.md dialog
box.
- To download the GUI for offline use, click the
icon in the GUI Composer application and
follow the prompts (see Figure 3-4).