SBOU299 May 2026
To set the device address, use the
following format: setdevice DEVID. Where setdevice
is always lower case, and DEVID is the four LSBs of the address in
decimal format (for example, for- an address of 0x4A, use 10).
Note that when the SCB is reset while one or more EVMs are connected, the address defaults to the lowest address found. The SCB checks for I2C or SPI at start up, if no device is attached, the SCB defaults to SPI. Reset the SCB with an I2C EVM connected to use I2C.
As an example, to set the INA233 with
a register address of 0x4A, send the command: setdevice 10. For
this example, the EVM returns the acknowledgment and states ("idle" or "collecting")
in JSON format: