The following instructions describe how to set up and use the EVM.
- Purchase an SCB.
- To use a PAMB Controller instead, see PAMB Compatibility.
- Download the following driver and install as an administrator: https://www.ti.com/lit/zip/sbac253.
- Follow the download prompts, a myTI™ account is required.
- Note that this driver is labeled as a PAMB driver,
but is also used for the SCB.
- Attach the EVM to the SCB Controller as shown in
Figure 3-1.
- Refer to Figure 3-2 when connecting multiple EVMs of the same type together.
- Connect the EVM to the PC using the provided USB cable.
- Insert the micro USB cable into the SCB Controller onboard USB receptacle J2.
- Plug the other end of the USB cable into a PC.
- Access the GUI from this link in either Chrome™, Firefox™,
or Safari™: https://dev.ti.com/gallery/info/CurrentSensing/INA233EVM_GUI/.
- Connect the GND reference of the external system to the GND node of the EVM (pin 1 of J1).
- Provide a differential input voltage signal to the
IN+ and IN– nodes by connecting the signal leads to J1 pin 5 or 6 and J1 pin 3
or 4 on the EVM as explained in Current Sensing
Operation.