To connect the GUI to the EVM, follow these steps:
- Setup and launch the GUI as described in Initial Setup.
- Make sure to connect the EVM to the SCB before
powering on.
- Close the README.md file page to initiate a
connection between the EVM and the GUI. If successful, the Hardware Connected
message is visible near the bottom-left corner of the GUI.
- A green indicator with the
device type and the text DEVICE CONNECTED is also visible near
the top left of the GUI.
- If the Hardware
Connected and DEVICE CONNECTED text do not show in the
GUI, long-press the reset (RST) button on the EVM to try again.
- If that option
does not work, check different hardware COM ports under
Options > Serial Port.
- If the hardware still does
not connect, check to make sure the correct GUI/EVM combination is being
used.
- If the correct
GUI/EVM combination is being used, the firmware of the SCB needs
to be reprogrammed as described in Firmware Debug.
- Many
connectivity issues can be addressed by performing one of the
following actions:
- Long-press the reset (RST) button on the EVM with the
EVM and SCB connected to each other.
- Refreshing the GUI can also sometimes help.
- Connect
the EVM to a different USB port.
- Avoid using long cables and USB hubs.
- If a desktop PC is being used, try a USB port on
the back.