SBOU316A September 2024 – June 2025
The INA630 is a monolithic precision instrumentation amplifier that incorporates an indirect current-feedback architecture. The gain is set by the ratio of two external resistors for a gain range of 20V/V to 1000V/V. The ratio gain set method allows for very low gain drift when a TC matched resistor network is used. The device has high precision as a result of super-beta input transistors, which provide low input offset voltage, offset voltage drift, input voltage noise, and current noise. The indirect current feedback architecture offers low gain error and non-linearity and the reference pin impedance does not degrade the common-mode rejection (CMRR) performance. For a full list of electrical characteristics for the INA630, see the INA630 Precision, Low-Power, Indirect Current Feedback Instrumentation Amplifier data sheet.
Figure 3-1 shows the full schematic of the INA630EVM. The components marked with a red X are optional and not installed. The purpose of these components is explained in subsequent sections of this document.