SBVS458A January 2025 – April 2025 TPS7B4261-Q1
PRODUCTION DATA
The device has an internal current limit circuit that protects the device during overcurrent or shorting conditions. The current-limit circuit, as shown in Figure 6-3, is a brick-wall scheme. When the device is in current limit, the device sources ICL and the output voltage is not regulated. In this scenario, the output voltage depends on the load impedance.
During current-limit events, the potential for high power dissipation exists because of the elevated current level and the increased input-to-output differential voltage (VIN – VOUT). If the heat dissipation is substantial, the device enters thermal shutdown. If the current-limit condition is not removed when the device turns back on after cooling, the device enters thermal shutdown again. This cycle continues until the current-limit condition is removed. The device survives this fault, but repeatedly operating in this mode degrades long-term reliability.
The current limit (ICL) for this device meets the specification provided in the Electrical Characteristics when the input voltage is VIN ≥ 3.7V. If the device output shorts to ground when operating in the range 3.3V ≤ VIN < 3.7V, current larger than ICL flows through the device. This behavior is described in Figure 5-19.