SBVS477A May 2025 – July 2025 TPS7B4259-Q1
PRODUCTION DATA
The TPS7B4259-Q1 has an open-drain based power-good pin that helps detect undervoltage and overvoltage fault conditions at the tracker output. Pull this pin up to a regulated rail (VPULL-UP) with a pullup resistor. Use the VPG range of values listed in the Recommended Operating Conditions table to determine the maximum value of the VPULL-UP regulated rail. Verify the input voltage VIN is higher than VUVLO (RISING) for VPG to have a valid value. VPG is the voltage of the power-good pin.
The power-good feature helps monitor the output voltage and detect possible fault conditions. This functionality is conditional on sufficient voltage being provided to the IN, ADJ, and EN pins. See the Recommended Operating Conditions table for the correct operating voltage ranges at these pins. The PG pin is pulled to VPULL-UP when the tracker output voltage remains within the VPG UV-TH and VPG OV-TH values of VADJ.
Variations in VOUT beyond the power-good switching thresholds lasting longer than tPG takes the PG pin low to a voltage of VPG < VPG, LOW. Transients in VOUT that last less than tPG are not flagged as errors by the PG pin. VOUT is the tracker output voltage. The PG pin remains low when the device is disabled (VEN < VEN, OFF), even if sufficient VIN and VADJ are provided. The values of VPG UV-TH, VPG OV-TH, tPG, and VPG, LOW are specified in the Electrical Characteristics table.