SCDS473 July 2025 TMUX9612
ADVANCE INFORMATION
TMUX9612 Truth Table shows the truth tables for the TMUX9612.
| SEL #(1) | CHANNEL # |
|---|---|
| 0 | Channel # OFF |
| 1 | Channel # ON |
If unused, then the SELx pins must be tied to GND or Logic High so that the devices do not consume additional current as highlighted in Implications of Slow or Floating CMOS Inputs. Unused signal path inputs (Sx or Dx) should be connected to GND for best performance.