SCDS473 July 2025 TMUX9612
ADVANCE INFORMATION
Bandwidth (BW) is defined as the range of frequencies that are attenuated by < 3dB when the input is applied to the source pin (Sx) of an on-channel, and the output is measured at the drain pin (Dx). Figure 7-8 and Equation 3 shows the setup used to measure bandwidth of the switch.