SCDS477A June 2024 – June 2025 TMUX1308A , TMUX1309A
PRODUCTION DATA
The TMUX1308A and TMUX1309A device have a transmission-gate topology. Any mismatch in capacitance between the NMOS and PMOS transistors results in a charge injected into the drain or source during the falling or rising edge of the gate signal. The amount of charge injected into the source or drain of the device is known as charge injection, and is denoted by the symbol QC. Figure 7-7 shows the setup used to measure charge injection from source (Sx) to drain (D).
Figure 7-7 Charge-Injection Measurement Setup