SDAA075 October 2025 CC2340R5
The following sections describe the hardware, which must be procured, setup changes implemented on the EVMs, and the necessary connections required to run the example without any modifications to the default firmware design.