SDAA183 December 2025 CC2340R5
Projects built inside of CCS can be loaded either directly in this IDE by selecting Run -> Flash Project (Ctrl + F5) or Debug Project (F5). It is recommended to exit Debug Mode to allow free-running if the project is not actively being debugged. Also consider using the Uniflash software tool to load binary images.
Figure 3-2 CCS Load Options