SDAA183 December 2025 CC2340R5
If USE_TEMP remains defined, this function will be called every TEMP_UPDATE µs to read the on-chip temperature sensor and return the result in °C, which is then assigned to the two seven-segment displays.