SDAA183 December 2025 CC2340R5
A 1/3 duty, 1/3 bias LCD with three COM and seven segment lines was selected as the demonstration for this document. As such, there are 21 individual LCD segments which can be controlled on this device including two seven-segment characters and seven single-segment ancillary symbols. Two additional control pins are required for the resistive network, and an additional pin is needed to drive the backlight. Thus the total number of GPIOs for controlling this LCD totals 13, and more would be needed for further LCD segment expansion.
Figure 1-2 Seven-Segment LCD Pin Array