SDAA378 August   2026 ADS125H18

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Detailed Description
    1. 2.1 Understanding ADS125H18 OWCS Operation
    2. 2.2 Using OWCS with Single-Ended Input Signals
      1. 2.2.1 Analyzing OWCS Behavior for Single-Ended Input Signals
      2. 2.2.2 Verifying OWCS Operation with a Single-Ended Input Using the ADS125H18EVM
        1. 2.2.2.1 Verifying OWCS Operation with a Single-Ended Input
        2. 2.2.2.2 Using a Fewer Number of Conversions for OWCS with a Single-Ended Input
          1. 2.2.2.2.1 Unsettled Data for Single-Ended Inputs
          2. 2.2.2.2.2 Settled Data for Single-Ended Inputs
        3. 2.2.2.3 How Input Capacitance Affects OWCS Performance for Single-Ended Inputs
        4. 2.2.2.4 Using the ADS125H18 Programmable Delay to Mitigate Settling Effects for Single-Ended Inputs
    3. 2.3 Using OWCS with Differential Input Signals
      1. 2.3.1 Analyzing OWCS Behavior for Differential Input Signals
      2. 2.3.2 Verifying OWCS Operation with a Differential Input Using the ADS125H18EVM
        1. 2.3.2.1 Verifying OWCS Operation with a Differential Input
        2. 2.3.2.2 Using a Fewer Number of Conversions for OWCS with a Differential Input
          1. 2.3.2.2.1 Unsettled Data for Differential Inputs
          2. 2.3.2.2.2 Settled Data for Differential Inputs
        3. 2.3.2.3 How Input Capacitance Affects OWCS Performance for Differential Inputs
          1. 2.3.2.3.1 Back-to-Back, Differential OWCS Measurements with Input Capacitance
        4. 2.3.2.4 Using the ADS125H18 Programmable Delay to Mitigate Settling Effects for Differential Inputs
    4. 2.4 Using the ADS125H18 Channel Sequencer to Implement an OWCS Algorithm
      1. 2.4.1 Example: Configuring the ADS125H18 Sequencer for the OWCS Algorithm
      2. 2.4.2 Understanding the OWCS Algorithm in the ADS125H18 Example Code
        1. 2.4.2.1 Initialization
          1. 2.4.2.1.1 Initialize the sequencer
          2. 2.4.2.1.2 Enter the "_step" Array Values
          3. 2.4.2.1.3 Analyze the Sequence
        2. 2.4.2.2 Starting the Sequencer and Processing Data
          1. 2.4.2.2.1 Update OWCS Step Values and Calculate "total_conversions"
          2. 2.4.2.2.2 Starting the Sequencer and Taking Data
          3. 2.4.2.2.3 Processing the OWCS Data
          4. 2.4.2.2.4 Using the OWCS Results
  6. 3Summary
  7. 4References
  8. 5Appendix A
    1. 5.1 Using OWCS with Redundant Systems
      1. 5.1.1 Dual, Redundant Systems versus Single-Device Systems
      2. 5.1.2 Using 1x OWCS versus 2x OWCS in a Dual Redundant System
      3. 5.1.3 Error Sources in Dual, Redundant Systems
        1. 5.1.3.1 RA1 and RB1 Errors
        2. 5.1.3.2 RA2 and RB2 Errors
        3. 5.1.3.3 VREF1 and VREF2 Errors
      4. 5.1.4 Measuring Differential Inputs in a Dual, Redundant System
      5. 5.1.5 Dual, Redundant System Summary

RA1 and RB1 Errors

Figure 5-5 plots the effect that a ±15% RA1 and RB1 resistance variation has on a dual, redundant system assuming RA2, RB2, VREF1, and VREF2 maintain their nominal values:

 OWCSDelta Behavior due to RA1 and RB1 Errors in a Dual, Redundant System (Single-Ended Input, ADS125H18V20)Figure 5-5 OWCSDelta Behavior due to RA1 and RB1 Errors in a Dual, Redundant System (Single-Ended Input, ADS125H18V20)

Figure 5-5 shows that a positive RA1 and RB1 resistance variation causes a significant positive shift (offset) in the threshold curve while a negative resistance variation causes a significant negative shift. However, Table 5-2 reveals that only a small difference exists between the minimum and maximum OWCSDelta_SE values despite the large offset. In other words, varying the RA1 and RB1 resistors causes a large shift in the OWCSDelta_SE values but a negligible change in the OWCSDelta_SE range.

Table 5-2 OWCSDelta Minimum and Maximum Values Due to RA1 and RB1 Errors in a Dual, Redundant System (Single-Ended Input, ADS125H18V20)
RA1 & RB1 variationOWCSDelta_SE (min)OWCSDelta_SE (max)Difference
-15%19.13%21.42%2.30%
Nominal22.50%25.00%2.50%
+15%25.88%28.55%2.67%