SDAA378 August 2026 ADS125H18
Section 2.2.2 describes the OWCS performance using the standard ADS125H18 EVM with no passive components installed between the terminal block and the ADC input pins. However, many industrial systems include capacitors on the inputs for noise rejection or other purposes. Figure 2-10 shows an example of a system with a differential capacitor in red installed between the AIN8 and AIN9 analog inputs as well as common-mode (single-ended) capacitors in blue installed between each input and ground. The ADS125H18 EVM includes footprints for these components that are not populated by default.
Adding capacitance on the analog inputs can help reduce noise at the expense of increased settling time due to capacitor charging. This behavior affects the measurement when the current sources (OWCS) switch on because the capacitor cannot charge up to the required voltage instantaneously. This effect is also measurable when the OWCS turn off because the capacitor cannot discharge instantaneously.
Multiple capacitors were installed on the ADS125H18 EVM to measure how input capacitance affects the OWCS detection behavior. Otherwise, the same settings were used as listed at the beginning of Section 2.2.2. The input was then measured by taking 512 conversions with the OWCS disabled followed by 512 conversions with the OWCS enabled. Next, the OWCSDelta_SE value was calculated using Equation 1 and converted to a predicted RSOURCE_OWCS value by rearranging the terms in Equation 7. Table 2-7 shows the measured, averaged results when RSOURCE = 800kΩ across 3 different ODRs and 4 different input capacitance values:
| Input capacitance (nF) | ODR = 1.6kSPS | ODR = 12.5kSPS | ODR = 50kSPS | ||||
|---|---|---|---|---|---|---|---|
| OWCSDelta_SE | RSOURCE_OWCS (kΩ) | OWCSDelta_SE | RSOURCE_OWCS (kΩ) | OWCSDelta_SE | RSOURCE_OWCS (kΩ) | ||
| 1 | 23.46% | 781.15 | 23.45% | 769.40 | 23.41% | 716.45 | |
| 10 | 23.42% | 731.64 | 23.33% | 616.85 | 23.19% | 480.98 | |
| 100 | 23.32% | 614.03 | 23.11% | 406.91 | 22.84% | 196.04 | |
| 1000 | 23.06% | 359.71 | 22.65% | 80.54 | 22.53% | 13.18 | |
Table 2-7 reveals that the OWCSDelta_SE values vary greatly across data rate and input capacitance. For example, the predicted RSOURCE_OWCS value when ODR = 1.6kSPS and input capacitance = 1nF is 781.15kΩ. This result is approximately equal to the ideal 800kΩ RSOURCE value. However, the predicted RSOURCE_OWCS value when ODR = 50kSPS and input capacitance = 1000nF is only 13.18kΩ! Reviewing the data point-by-point helps illuminate why such a large discrepancy exists across the different parameters.
Figure 2-11 plots the OWCSDelta_SE values point-by-point for RSOURCE = 800kΩ and ODR = 12.5kSPS for 4 different input capacitance values: 1nF, 10nF, 100nF, and 1000nF.
Figure 2-11 reveals the significant effect input capacitance has on the OWCS behavior as well as why there is such extreme variation in the results listed in Table 2-7:
These conclusions make sense because the capacitor time constant increases as the input capacitance increases, resulting in longer settling times.
Changing the ODR with input capacitors installed also affects the OWCS performance as mentioned previously. Figure 2-12 plots the OWCSDelta_SE values for RSOURCE = 800kΩ and input capacitance = 10nF point-by-point for 3 different ODRs: 1.6kSPS, 12.5kSPS, and 50kSPS. The plot x-axis units are in milliseconds to clearly indicate the charging behavior captured by the ADC. Also, all plots start at the same point and overlay each other.
The results in Figure 2-12 make sense because the ADC sampling time decreases as ODR increases, even though the capacitor time constant remains unchanged. Therefore, the ADC captures more of the capacitor charging behavior and less of the steady-state behavior as the data rate increases, leading to less stable measurements.
The input capacitance does help reduce noise as stated previously. Figure 2-13 plots the measured ADC code point-by-point with OWCS disabled for RSOURCE = 800kΩ and ODR = 12.5kSPS for 4 different values of input capacitance: 1nF, 10nF, 100nF, and 1000nF.
Figure 2-13 qualitatively shows that the noise spread decreases as the input capacitance increases. Specifically, the RMS noise when input capacitance = 1nF is 160.38 codes, while the RMS noise when the input capacitance = 1000nF is only 14.09 codes. Designers must take care to balance the noise reduction benefits of an input capacitor with the challenges introduced by capacitor settling.