SDAA378 August 2026 ADS125H18
Figure 2-33 shows an example system that measures both input signals and monitoring signals as follows:
Moreover, Figure 2-33 highlights the ADS125H18 OWCS feature and associated multiplexer in green:
Figure 2-34 uses the format shown in Figure 2-32 to demonstrate how to setup the sequencer for the example system in Figure 2-33. All information shown in Figure 2-34 can be stored in the ADS125H18 sequencer and was arbitrarily chosen for this example.
Interpret Figure 2-34 as follows:
For example, Step 13 measures ten conversions between inputs AIN15 and RESN. Note that the ADS125H18 sequencer allows the user to configure many other parameters on a per-step basis; however these parameters are not necessarily relevant to the OWCS algorithm and are not discussed further in this document.
Figure 2-34 also shows that the "Channel" for the OWCS steps in green are to be determined, or TBD. These settings are initially TBD because they change from one sequence to the next. However, the input steps and monitoring steps remain unchanged. Figure 2-35 shows how to configure the OWCS steps during the first sequence: the first and second OWCS steps (#25 and #26, respectively) are both configured with AIN0-RESN because this is the same channel used in the first sequence step (#4). Important settings for the first sequence step are highlighted in yellow.
Start the sequencer by setting the START bit or toggling the START pin. The ADS125H18 sequencer indexes through each step in Figure 2-35 from left to right and measures 129 total conversions. The user must decide how to use the information received from each input and monitoring step, as well calculate the OWCS threshold.
Reconfigure the OWCS steps before the next sequence starts if necessary. Figure 2-36 shows how to configure the OWCS steps during the second sequence: the first and second OWCS steps (#25 and #26, respectively) are both configured with AIN4-RESN while the third and fourth OWCS steps (#27 and #28, respectively) are both configured with AIN5-RESN. These settings are required because the second step (#7) measures a differential input but the OWCS feature must always measure single-ended channels. Important settings for the second sequence step are highlighted in yellow.
Again, start the sequencer by setting the START bit or toggling the START pin. The ADS125H18 sequencer indexes through each step in Figure 2-36 from left to right and measures 153 total conversions because the last two OWCS steps are enabled in this sequence. The user must decide how to use the information received from the input and monitoring steps, as well as calculate the OWCS threshold for each single-ended input. Ideally, the calculated OWCS result for AIN4-RESN should be identical to the OWCS result for AIN5-RESN because this is a differential measurement.
Figure 2-37 follows the same logic to show how to reconfigure the OWCS channels before starting each of the next three sequences such that all input step channels in blue are analyzed for wire breaks. Important settings per sequence are highlighted in yellow.
All input step channels have been diagnosed for wire breaks using the OWCS after sequence 5 completes. At this point, the user should reconfigure the OWCS channels to wrap back around to the first input step channel as shown in Figure 2-35, restarting the complete process. The user then decides how many total sequences to run as well as what to do if they detect a wire break.