SDAA378 August 2026 ADS125H18
Table 2-4 shows an average OWCSDelta_SE value calculated using 512 samples with OWCS disabled and 512 samples with OWCS enabled. Section 2.2.2.1 states that 512 conversions per sequence step were used to capture any possible settling behavior. However, taking a total of 1024 conversions to detect a single wire break might require an impractical amount of time in many industrial systems. For example, 1024 conversions at 1.6kSPS takes approximately 640ms. Analyzing the sampled data points helps indicate how many conversions are actually necessary for accurate fault detection.
Figure 2-8 plots the OWCSDelta_SE values point-by-point instead of a single value averaged over 512 conversions as listed in Table 2-4. Figure 2-8 uses RSOURCE = 500kΩ and 3 different ODR values: 1.6kSPS, 12.5kSPS, and 50kSPS
Figure 2-8 reveals that some settling behavior exists in the data, but otherwise very little useful information due to the unsettled outlier. Breaking this data into unsettled and settled components helps clarify why fault detection errors might occur. Also, note that this behavior is shown at RSOURCE = 500kΩ but exists across all values of RSOURCE.