SDAA378 August 2026 ADS125H18
This section analyzes the behavior of the OWCS when a single-ended input with source impedance RSOURCE is applied to the ADS125H18. Figure 2-2 shows the circuit used to analyze a single-ended input with the OWCS disabled and a single-ended RSOURCE impedance:
The ADC measures the single-ended voltage difference between nodes VAIN0 and VRESN in Figure 2-2 such that Equation 1 can be expanded to Equation 3:
Use superposition to analyze the voltage contribution from each source in the circuit by shorting voltage sources or opening current sources. For example, Figure 2-3 shows that calculating the total voltage at AIN0 with the OWCS enabled, V(AIN0)OWCS_SE, requires three different superposition configurations:
Table 2-2 describes each nodal voltage after applying this same analysis to every term in Equation 3:
| Voltage term | Nodal voltages |
|---|---|
| V(AIN0)OWCS_on | = V(AIN0)AIN0_AVDD_SE + V(AIN0)RESN_AVDD_SE + V(AIN0)AIN0_OWCS_SE where
|
| V(RESN)OWCS_on | = V(RESN)AIN0_AVDD_SE + V(RESN)RESN_AVDD_SE + V(RESN)AIN0_OWCS_SE where
|
| V(AIN0)OWCS_off | = V(AIN0)AIN0_AVDD_SE + V(AIN0)RESN_AVDD_SE where
|
| V(RESN)OWCS_off | = V(RESN)AIN0_AVDD_SE + V(RESN)RESN_AVDD_SE where
|
Importantly, Table 2-2 reveals that virtually all nodal voltages are identical such that Equation 3 can be reduced to Equation 4:
Figure 2-4 shows the superposition configurations for the terms in Equation 4:
Figure 2-4 also shows that the voltage at RESN with OWCS enabled, V(RESN)OWCS_SE, is 0V because the RESN pin is grounded. Therefore, Equation 4 reduces to Equation 5, which is represented by Figure 2-4 (left):
Equation 6 rewrites V(AIN0)OWCS_SE in Figure 2-4 (left) in terms of resistances RA, RB, and RSOURCE as well as current IOWCS:
Recall from Equation 2 that the actual OWCS current, IOWCS, is relative to the reference voltage, VREF. Therefore, the IOWCS term in Equation 6 can be rewritten in terms of the nominal OWCS current, IOWCS_NOM, and simplified as shown in Equation 7:
Equation 7 can also be rewritten to predict the single-ended RSOURCE_OWCS value from the measured OWCSDelta threshold, as shown in Equation 8:
Table 2-1 includes RB and IOWCS_NOM values for all ADS125H18 versions. Figure 2-5 applies all possible parameters from Table 2-1 to Equation 7 and sweeps RSOURCE from 1kΩ to 1GΩ to generate the ideal OWCSDelta_SE curves:
Figure 2-5 reveals two important takeaways for single-ended OWCS measurements:
| ADS125H18 version | Attenuation factor | OWCSDelta_SE Min | OWCSDelta_SE Max | Difference |
|---|---|---|---|---|
| V12 | 7 | 16.07% | 18.75% | 2.68% |
| V20 | 10 | 22.50% | 25.00% | 2.5% |
| V40 | 19 | 23.68% | 25.00% | 1.32% |