SDAA401 June 2026 ISOW1050 , ISOW3080 , ISOW6441 , ISOW6442 , ISOW6442-Q1
Using Y-capacitors on the printed circuit board (PCB) introduces lead inductance on both sides of the capacitor, in addition to the parasitic inductance of the capacitor, making the capacitor ineffective at frequencies higher than 200MHz. One way to create a low-inductance capacitance is by overlapping the internal PCB layers. This can be possible by a multilayer PCB layout. Extending the internal reference layers (GND and VCC) on either side of the isolation barrier (as shown in Figure 2-3) creates an overlap of internal layers. This overlap area, formed by the extension of the GND1 and VCC2 layers with FR4 material between the layers acting as a dielectric, creates a stitching capacitance between GND1 and VCC2.
Depending on whether the isolation requirement is functional, basic, or reinforced and depending on the working voltage, the spacing between the layers can be adjusted to achieve the capacitance value. Refer to the Low-Emission Designs With ISOW7841 Integrated Signal application report for an interlayer capacitance design example.
Figure 2-3 Diagram Showing Interlayer Capacitance Using PCB
LayersExtra care must be given at the edges of the PCB. At the edges, the planes can be exposed to air. Since opposite voltages come close to the edge of the board, these opposing voltages can potentially lead to electric field stress and then air breakdown along the edge.