SDAA401 June 2026 ISOW1050 , ISOW3080 , ISOW6441 , ISOW6442 , ISOW6442-Q1
Isolated transceivers (ISOWRS485 – ISOW3080 and ISOWCAN – ISOW1050) have isolated output buses that connect through cables to external devices. The cables or wires connected to the system can pick up high-frequency switching noise from the converter and act as transmitter antennas; longer cables result in higher radiation levels. The answer to this outcome is to keep the common-mode current loop as small as possible by using common-mode chokes (CMC), which can be used for attenuating the common-mode noise. A CMC (for example, the ACT45B-101-2P-TL003, see references, and L10 in Figure 2-1) offers high impedance to common-mode currents while passing differential signals with minimal insertion loss. As a result, common mode noise from the ISOW output is blocked before reaching the cable; the differential data signal passes unaffected.
Position of the CMC is crucial—if the CMC is placed far from the connector, common mode noise gets coupled into PCB traces which defeats the purpose of the choke. For layout guidelines to follow for minimizing stray fringe capacitance between the choke terminals, refer to Figure 2-2. Refer to the ISOW1050DWEEVM evaluation module for a detailed layout.