SDAA403 June 2026 TIC12400-Q1
The /INT pin is an active-low, open-drain output. It is normally held high by an external pull-up resistor connected to VDD and pulled low by the TIC12400-Q1 to assert an interrupt.
A common application concern is whether leakage current on the /INT pin could cause spurious triggering when the pin is in the de-asserted (high) state. The relevant datasheet parameter is the /INT output leakage current, tested with /INT pulled up to VDD:
| Parameter | Min | Max | Unit |
| /INT output leakage current (pin pulled up to VDD) | −1 | +1 | μA |
Table 4. /INT Pin Leakage Current Specification
The ±1 μA specification is a passing ATE parameter. In practice, the leakage current on the /INT pin is well within this range and is not a source of spurious interrupt triggering under normal operating conditions. The leakage current is three orders of magnitude smaller than the INx pin leakage (up to ±110 μA) and should not be confused with it.
NOTE: The ±110 μA leakage specification applies to the INx input pins only, not to the /INT output pin. These two specifications are independent and serve different design purposes.