SDAA403 June 2026 TIC12400-Q1
A specific edge case arises when the TIC12400-Q1 is used to detect a wakeup signal that may have already occurred before or during the device startup sequence. Because the first polling cycle establishes the baseline, any INx pin that is already in its "active" state when the first polling cycle completes will have that active state stored as the baseline value. No interrupt will be generated for a transition that was captured as the initial state.
Consider a case where a wake signal drives an INx pin HIGH during the period between power-on and the first polling cycle completing. The TIC12400-Q1 will store HIGH as the baseline for that channel. If the signal is later removed (going LOW), the device will detect the HIGH-to-LOW transition and assert /INT as expected. However, the initial HIGH-to-active transition will have been missed from an interrupt perspective.
To avoid missed wakeup signals in latency-sensitive designs, consider the following: