SDAA489 August   2026 TMCS2100-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Quick-Start Design Checklist
  6. 3Bus Bar Design
    1. 3.1 Straight Bus Bar
    2. 3.2 Bus Bars with a Bend
  7. 4Surrounding Conductors / Magnetic Materials
    1. 4.1 Straight Bus Bar
    2. 4.2 Bus Bars with a Bend
    3. 4.3 Ambient Fields
  8. 5PCB Cutouts
  9. 6Device Placement
    1. 6.1 Field Strength
      1. 6.1.1 Distance from Bus Bar to Sensor
      2. 6.1.2 Sensor-to-Sensor Spacing
      3. 6.1.3 Full-Scale Range and Device Gain Variants
        1. 6.1.3.1 Device Gain Variants
        2. 6.1.3.2 Full-Scale Range
        3. 6.1.3.3 Plot Similarities
      4. 6.1.4 Gain Considerations
  10. 7Simulation Tools
    1. 7.1 DC Simulation Tool
    2. 7.2 AC Simulation Tool
  11. 8Characterization Requirements
  12. 9References

Device Placement

The TMCS2100-Q1 is an ambient magnetic field sensor. Device placement on a PCB relative to the current-carrying bus bar is important to ensure that the sensors see a sufficient amount of magnetic field. The placement of the devices also has an impact on displacement error.