SDAA489 August 2026 TMCS2100-Q1
When simulating it is important to find a location where the Gain 2 values for each device remain less than 16128. This provides headroom for two critical functions: frequency compensation circuitry to correct amplitude errors that grow with frequency, and tolerance margin to account for differences between the simplified 2D DC simulation model and real 3D bus bar geometry, PCB stack-up variations, and assembly tolerance. Systems with Gain 2 values exceeding 16128 leave no buffer for these corrections, which can result in frequency-dependent errors that cannot be corrected by the TMCS2100-Q1's frequency compensation scheme. If sensor placement results in high Gain 2 values, consider moving the sensors closer to the bus bar to increase gain margin, or select a higher-gain device variant (A2 or A3) to reduce the overall gain requirement.