SFFSAY3 January 2026 F29H850DM , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P589DM-Q1 , F29P589DU-Q1 , TMCS1123 , TMCS1123-Q1 , TPS650362-Q1 , TPS650364-Q1 , TPS650365-Q1 , TPS650366-Q1
Prior to conducting the HARA, the following simplifying assumptions are adopted to limit the analysis scope:
Once the functions, processes, and interactions of each item have been defined, the next phase is the HARA. Using the assumptions and analyses already established, any incorrect behavior in each subsystem can give rise to potential hazard events, such as DC overvoltage, DC bus overcurrent and thermal failure.
Each hazard must be evaluated separately using the ISO 26262: 2018 criteria of Severity (S), Exposure (E) and Controllability (C). Take thermal failure as an example:
According to Table 1-3, the combination S3 – E3 – C2 corresponds to ASIL‑B, so the thermal‑failure hazard is assigned ASIL‑B.
Regarding DC bus overcurrent, it will not have a significant impact on the high-voltage battery, because the maximum charging current of the high-voltage battery is much higher than the current of AC charging. However, overcurrent can cause the power devices on the OBC output side to overheat and fail due to short circuits. Following a short-circuit failure, the high-voltage battery can create a low-impedance pathway through the OBC, potentially resulting in severe system overheating and, in extreme cases, vehicle fires. The exposure and controllability level are the same as thermal failure. According to Table 1-3, the combination S3 – E3 – C2 corresponds to ASIL‑B, so the DC bus overcurrent hazard is assigned ASIL‑B.
For DC bus overvoltage, it can cause overvoltage breakdown of the power devices on the OBC output side, and overvoltage is also hazardous to Li-ion cells on high-voltage battery, which can further lead to system overheating or even vehicle fire. The exposure and controllability level are the same as thermal failure. According to Table 1-3, the combination S3 – E3 – C2 corresponds to ASIL‑B, so the DC bus overvoltage hazard is assigned ASIL‑B.
All hazard events need to be analyzed. Since this assessment is typically performed by the system integrator, the detailed evaluation of every hazard is not presented here. HAZOP is a system hazard analysis method, which can provide 7 guide words. Table 2-7 illustrates an example of the HARA analysis. HAZOP leading word is used in malfunction behavior.
| ID | Malfunction Behavior | Potential Vehicle Level Hazard | S | E | C | ASIL |
|---|---|---|---|---|---|---|
| H1 | More thermal than expected | Vehicle fire caused by overheating | S3 | E3 | C2 | B |
| H2 | More DC bus current than requested | Vehicle fire caused by OBC short-circuit | S3 | E3 | C2 | B |
| H3 | More DC bus voltage than requested | Vehicle fire caused by OBC short-circuit | S3 | E3 | C2 | B |
| H4 | More electrical interference | Spurious control signals | S1 | E3 | C2 | QM |
For hazard events from ASIL A to ASIL D in Table 2-7, at least one safety goal must be identified. A functional‑safety goal is a high‑level, technology‑independent statement that fulfills the safe state requirement.
Table 2-8 is an example entry of FuSa goal. The FTTI value must be derived from hazard analysis and regulatory requirements. Take SG1 as an example, the operating temperature is 65 °C, and the thermal failure critical temperature is 155 °C. With general temperature rise rate 15 °C / s, the time to critical temperature is 6s. 500ms FTTI time is conservative for early detection to allow early intervention before cascading failure.
| ID | Safety Goal | ASIL | Safety State | FTTI |
|---|---|---|---|---|
| SG1 | Avoid vehicle fire due to thermal failure. | B | OBC shutdown, and switch to emergency operation mode. | Specified by users |
| SG2 | Avoid vehicle fire due to DC bus overcurrent. | B | ||
| SG3 | Avoid vehicle fire due to DC bus overvoltage. | B |
The safe state requirement states the system‑wide response that must be triggered when the hazard occurs. For example, the safe state of SG1 to SG3 is that OBC shall be switched into emergency operation mode, in which key actions are shown as below. Different from dual-stage OBC, this architecture does not contain a DC‑link capacitor, so there is no action on discharging DC-link capacitor.