SLAA450G April 2010 – April 2020
After the LaunchPad is connected to the host, it needs to be determined which COM port it is assigned to.
On Windows® XP systems, this can be determined by using Device Manager. Device Manager can be started by running devmgmt.msc.
Figure 4. Screenshot of Windows® XP Device Manager In the section named Ports (COM & LPT), the LaunchPad should show up as MSP430 Application UART. The COM port number is shown to the right of this name. In Figure 4, for example, the port number is COM11.